Cybersecurity
SACE Emax 3 CyberSecure is a specific configuration of SACE Emax 3 (factory-fitted) that restricts write access exclusively to authorized users via the tools.
This configuration differs from the current practices of other ABB devices, where the permitted operations are contingent upon the user's direct role within the tools.
In his regard, novel "Device-Centric" roles have been introduced, which are exclusively designed to impact the physical device for which they are intended.
Roles
SACE Emax 3 CyberSecure is a specific configuration of SACE Emax 3 (factory-fitted) that restricts write access exclusively to authorized users via the tools.
This configuration differs from the current practices of other ABB devices, where the permitted operations are contingent upon the user's direct role within the tools.
In his regard, novel "Device-Centric" roles have been introduced, which are exclusively designed to impact the physical device for which they are intended.
- The "Owner" role is a unique and powerful position that controls the breaker’s protection settings and advanced features. This role can assign roles to others, remove users, and is exclusive to one individual per breaker.
- An "Admin" is a key role that not only oversees the protection settings and advanced features of circuit breakers but also has the authority to delegate roles to other users. This role is pivotal in maintaining system integrity and managing user access.
- An "Engineer" is entrusted with the responsibility of managing the protection settings of circuit breakers and utilizing their advanced features in the Tools section. This role involves enhancing system efficiency and ensuring safety through these settings and functionalities.
- An "Operator" is in charge of controlling the safety measures of a circuit breaker, performing basic operations and tests. They can access and modify its fundamental features to guarantee maximum efficiency and security.
- A "Viewer" is meant for users to see all settings and information within a system without the ability to make any changes. This role is designed for those who need to stay informed without having the ability to alter any configurations or data.