Useful information

Operating mode

The device can be in one of the following operating modes:
  • local: configuration via Ekip T&P or Ekip Programming is enabled. In general, this is the mode for the first configuration of the device, which also includes the configuration of the device in relation to the installation in which it is installed.
  • remote: configuration via Ekip T&P or Ekip Programming is disabled. In general, this is the mode that allows remote control and configuration of the release and protection function parameters.
The current operating mode is shown on page Information.