Read the previous article
Become an Owner
Based on the role the user has for a given device, he will have a series of actions that he can perform on the device, regardless of whether it is connected to the PC or not.
| Action | Description |
|---|---|
| Become Owner | If the device does not yet have an owner, the user can ask to obtain the role. It is required to be connected to the device and have an internet connection. |
| Contact Owner | If the device has an owner, it is possible to send him a request. |
| See users list | If the user has an Owner / Admin role, it is possible to consult the list of users who have a role for the selected device. |
| Add a user | If the user has an Owner / Admin role, it is possible to assign a role to a user. |
| Edit a user | If the user has an Owner / Admin role, it is possible to edit the role assigned to a user. |
| Delete a user | If the user has an Owner / Admin role, it is possible to delete the role assigned to a user. |
| Transfer the Ownership | If the user is the Owner of a device, it is possible to transfer the Ownership to another user with Admin role. |
| Accept / Decline the Ownership | If the user was designated to became the new Owner of a device, it is possible to accept or decline the request. |