Communication

Page functions

  • Configure Internet connection parameters.
  • Configure the parameters for Ethernet or Modbus communication with the devices.
  • Monitor the list of clients connected to the device.
 

What it looks like

communication gateway
 
PartDescription
A

Communication pages menu:

  • Parameters: displays the parameters for communication with the Internet and for Ethernet or Modbus communication with the devices.
  • Clients: displays the list of clients connected to the gateway.
BModbus communication parameters
CInternet connection parameters
DEthernet communication parameters
 

Actions on the page

ButtonAction
DiscardCancels the changes
SaveTransfers configuration to the device
 
Configure communication with the Internet
In the Parameters tab, set the Ethernet parameters in LAN 1: the parameters are saved automatically.
 
Configure communication with devices
  • In the Parameters tab, set the parameters for the Modbus or Ethernet ports in LAN 2.
  • To transfer the configuration to the device, click on the relevant button Save.