Protections

Page functions

  • Enable and configure two protection configuration sets.
 

What it looks like
protection page

 
protection page
 
PartDescription
A

Menu to select the set of protections to be configured

  • Settings A
  • Settings B
B
Trade-name of device
Customised device name (parameter CB Tag name editable in Classic view > Unit configuration > Customisable information)
Photo of the device
information icon : if available, opens a document with a sales presentation of the device.
C

List of available device protections. The following data are shown for each protection:

  • protection name
  • protection status
    • active icon: active
    • inactive icon: inactive
DProtection selected for the configuration
EConfiguration parameters for the selected protection
FButton to apply or cancel changes
 

Configure a protection

  1. To configure a protection of set B, click on Settings B.
  2. Click on the protection to be configured: the area containing the protection parameters appears.
  3. Enter the parameters.
  4. To transfer the configuration to the device, click on Apply: a message appears with the result of the operation.
Note: if the operation fails, check the status of the operating mode (Operating mode).