Area of parameter specific to the parameter category selected in A : expands all parameter sections. : collapses all parameter sections. : copies parameters and values to the clipboard. : exports parameters and values to .xls. : reads the saved values from the device. : writes the set values to the device.
C
Descriptor file in use
Edit a parameter
To view all parameters, click on .
To read the saved values from the device, click on .
Set the desired value or option.
To transfer the set values to the device, click on : a message appears with the result of the operation.
Note: if the operation fails, check the status of the operating mode (Operating mode).