Safety information

General information

 
WARNING! Dangerous voltage that can cause electric shock, burns or death. Do not handle, install, use or service this product until you have read the instructions.
WARNING! PLEASE READ THIS DOCUMENT CAREFULLY BEFORE INSTALLING AND USING THIS SOFTWARE WITH THE DEVICES THAT CAN BE CONFIGURED AND MONITORED.
These instructions must be archived along with any other instructions, drawings and descriptive documents. Keep this document in an accessible place for consultation when required.
Consult the manuals of the connected devices when installing the software. This software is designed to function in accordance with the compatibility specifications. Consult the relative section before use.
The software must be used by qualified personnel who have read all the installation instructions. Follow the safety procedures indicated by your company and make sure that the devices are in safe conditions according to regulations.
Do not touch covers, open doors or work on the apparatus connected to the software unless the power supplied to the switchboard in which it is housed has been disconnected and before all the circuits have been de-energized.
Before carrying out checks, visual inspections and tests on the device, disconnect all power and voltage supplies.
 

Information for circuit breakers

DANGER! The following operations are mandatory before proceeding with any work on a circuit-breaker:
  1. Open the circuit breaker and make sure that the springs of the operating mechanism are not loaded (if applicable).
  2. Disconnect the circuit breaker (power circuit and auxiliary circuits) from the electric power source and earth the terminals in a visible way, on both the supply side and load side.
  3. Detach the circuit breaker from the installation. Remove it from the switchgear if possible.
  4. Put equipment in a safe condition as established by the standards and laws in force.
 

CAUTION!

  • This document does not contain the detailed descriptions of each page available when each compatible device is connected, the safety regulations or the possible interactions with the maintenance operations. Please note that this document contains warnings and precautionary instructions, but does not envisage all the possible modes in which the software can be used and that may or may not be recommended by ABB, nor the possible risks that each of these modes implies, neither can ABB investigate these issues. Anyone who implements procedures or uses equipment that may or may not be recommended by ABB must make very sure that neither the safety of the personnel nor that of the installation is endangered by the chosen procedures or equipment. Please contact ABB if further information is required or if specific problems arise that have not been explained sufficiently.
  • This document is designed for use by qualified personnel. It is not intended as a substitute for an adequate training course or adequate experience with the safety procedures of this software connected to the equipment.
  • It is the responsibility of the Customer, the installer or the end user to make sure that warning signs are affixed and that all the access doors and operating handles are closed in safety conditions when the equipment connected to the software is left even only momentarily unattended.
  • All information in this document is based on the latest product data available at the time of printing. ABB reserves the right to make changes at any time and without prior notice.

 

Information for the Modbus protocol

Security Disclaimer 

The Modbus protocol, by design, does not include any built-in security mechanisms. It lacks authentication, encryption, and integrity checks, making it inherently vulnerable to various cybersecurity threats, including unauthorized access, data interception, spoofing, and command injection. Modbus communications, especially over TCP/IP networks, can be easily intercepted or manipulated if not properly secured by external means.

 

Warning: Use of Modbus in unsecured or publicly accessible networks is strongly discouraged. It is recommended to implement compensating security controls such as network segmentation, firewalls, VPNs, intrusion detection systems (IDS), and access control mechanisms. Where possible, consider using secure alternatives or encapsulating Modbus within encrypted channels (e.g., Modbus over TLS).

This protocol should only be used in trusted environments or in conjunction with robust cybersecurity practices. Users are responsible for assessing the risks and implementing appropriate safeguards.

Modbus Protocol Mitigation

Since Modbus lacks built-in security, implement the following controls:

Network Segmentation

• Isolate device networks from enterprise networks with firewalls

• Use VLANs to separate control networks from management networks

• Only authorised engineers access device networks

• Restrict network access to specific MAC addresses (whitelisting)

Encrypted Remote Access

• Use VPN tunnels for all remote access to device networks

• Enable VPN authentication with strong credentials

• Disable direct internet access to device networks

• Consider Modbus over TLS if supported by devices

Firewall Controls

• Allow Modbus TCP (port 502) only from authorised workstations

• Allow TFTP (port 69) only during scheduled firmware updates

• Block all other inbound traffic on device networks

• Enable stateful inspection on firewall

Access Control

• Only Digital User role and higher can access devices

• Regular access reviews - remove unused accounts

• Log all authentication attempts

Monitoring & Detection

• Enable network intrusion detection on device networks

• Monitor for anomalous Modbus traffic patterns

• Alert on failed authentication attempts

• Review logs weekly for suspicious activity

Update Security

• Download firmware only from official ABB servers (HTTPS)

• Verify digital signatures before firmware installation

• Test firmware in lab environment before production deployment

• Document all firmware updates with date and user