This page let the user configure additional modules of the device by selecting the Communication or the Signalling modules.
Communication modules
Part
Description
A
Button to return to the main page with the additional module types
B
Menu with the available modules of the type selected
Note: the modules appear if the auxiliary power supply is present on the Ekip Supply module and if the “Local bus” parameter is enabled. Please refer to the device manual for information on enabling it.
C
Module data
D
Status: module status information Configuration: module configuration parameters
E
Button to confirm or cancel the change
Signalling modules
Note: the page that appears after selecting the Signal button is described below.
Part
Description
A
Button to return to the main page with the additional module types
B
Menu with the available modules of the type selected
C
Area for input and output parameters
Status: commands to enable or disable an input/output
Configuration: parameters to configure an input/output
D
Signal reset: button to reset the signal
Start autotest: button to start lighting up the LEDs on the module to check whether the inputs/outputs are enabled
Note: function only available if the operating mode status is Local (Information).
E
Button to confirm or cancel the change
Configure an additional module
Click on the button corresponding to the type of module to be configured (CommunicationorSignal).
Note: only buttons corresponding to module types physically installed on the device are enabled
If there are several modules, select the module you want to configure.
Enter the parameters.
To transfer the configuration to the device, click on Apply: a message appears with the result of the operation.
Note: if the operation fails, check the status of the operating mode (Operating mode).