Ekip Connect is ABB’s software for interfacing ABB-compatible low-voltage devices via computer. It allows you to configure, monitor, control and test devices.
Ekip Connect can connect to devices via USB, serial network or Ethernet network. Connection is made via the front test connector, or via communication modules installed on the device.
Note: Some device models can only be configured with Ekip Connect
Ekip Connect functions
Ekip Connect, depending on the device, can perform the following main functions:
Monitor the status of the connected device and record information.
Execute the operation, reset, signalling commands, etc.
Configure protection releases and devices with customised parameters and logic.
Download information from releases equipped with Data logger.
Create communication reports.
Save and restore configurations.
Perform tests on releases.
Update firmware of connected devices, modules and accessories.
View, manage and activate software packages from ABB Marketplace to enable new functionality on devices.
Interface
Area
Description
A
Scanning: page to scan devices (Introduction). Devices: list of devices detected by the scan allowing you to select another device to communicate with without moving from the current page.
B
Summary information of the communicating device:
Customised device name (parameter CB Tag name editable in Classic view > Unit configuration > Customisable information)
Device type (parameter CB Type also visible in Classic view > Information > General parameters)
Device family identifier
Device status:
: found but connection not yet established
/ (alternately): connected and operating normally
/ (alternately): connected but with active alarms
: disconnected
C
Pages available for the communicating device (Communication with devices). Note: the pages are displayed only if there is a device communicating.
D
Marketplace: page to purchase, view and install software packages for the device (Marketplace). Tools: page for access to Ekip Connect tools.
E
Top bar with buttons:
: to leave a feedback
: to authenticate yourself, find out the enabled role and duration, request a role and disconnect.
: to open the notification area for updates, news, bug fixing, discounts and marketplace opportunities.
: to open the help manual to see documentation
: to open the software settings menu, in particular: