Connectivity

Connectivity page functions

  • Enable/Disable gateway Ethernet/Wi-Fi communication.
 

Page To Internet

connectivity gateway
 
PartDescription
APages menu
BInternet connection type buttons available
 

Page To Internet > network

Internet gateway
 
Part
Function
BackReturns to the page with the connection type buttons.
Discard
Cancels the changes.
SaveTransfers the configuration to the device.
 

Page To Internet > Wi-Fi

wi-fi gateway
 
PartFunction
BackReturns to the page with the connection type buttons.
DiscardCancels the changes.
SaveTransfers the configuration to the device.
 

Page To Internet > Cellular

Internet cellular
 
PartFunction
BackReturns to the page with the connection type buttons.
DiscardCancels the changes.
SaveTransfers the configuration to the device.
 

Page To devices

Page to devices
 
PartFunction
AConnectivity pages menu
BConfiguration parameters:
Discard: cancels the changes.
Save: transfers the configuration to the device.
 

Enable and configure an Internet communication type

  1. In the To Internet tab, click on the button for the communication type to be enabled.
  2. Proceed as follows:
To communicate via...
Then...
network
  1. Set the communication parameters.
  2. To transfer the configuration to the device, click on Save.
Wi-Fi
  1. Select the desired Wi-Fi network from the list.
  2. Enter the password and type of authentication.
  3. Click on Connect.
  4. Click on Back: the message Actual connection appears at the bottom of the button relating to the type of communication enabled.
Cellular (3G/4G)
  1. Set the communication parameters.
  2. To transfer the configuration to the device, click on Save.
  3. To enable the connection, click on Connect.
  4. Click on Back: the message Actual connection appears at the bottom of the button relating to the type of communication enabled.
 

Disable an Internet communication type

  1. In the To Internet tab, position the cursor on the button relating to the type of communication to be disabled: the Disable button appears at the top right of the button.
  2. Click on Disable.
 

Enable and configure communication with devices

  1. Click on To devices.
  2. Set the communication parameters.
  3. To transfer the configuration to the device, click on Save.