Path in Classic view: Classic view > Datalogger
The function Datalogger allows the recording of data associated with a trigger event. The data recorded are:
download the recording to analyze it with function Data Viewer
>> For more details on supported devices and requirements for each, please refer to document 9AKK108467A9238 available here.
| Part | Description |
|---|---|
| A | Button to go back to the menu Tools |
| B | Tool layout where Datalogger operations may be executed. |
| Part | Description |
|---|---|
| A | Tooltip button area Start: Button to start datalogger recording Stop: Button to finalize the running datalogger recording. Download: Button to download the recorded datalogger. This button is only enable if datalogger is stopped. |
| B | Download Options: Options button to enable datalogger and set parameters about the recording (number of register, sampling frequency, stop delay). |
| C | Dynamic label to inform user about the status of datalogger. The available status are ready, running and stopped. |
Configuration is mainly done in the "Options" window which is reached via "Download options" button from tooltip.
Options window mainly consisted of 2 parts ; "General" and "Trigger" sections.
In section "General", enabling of function and usual configuration for the datalogger is managed. User decides the number of the register in sample, sampling frequency and stop delay for that datalogger record.
| Element | Description |
|---|---|
| Datalogger enabled | A button to enable/disable datalogger functionality |
| Number of register in sample | Number of register in sample (8, 16, 32) |
| Sampling frequency | Frequency of data collection. The higher the sampling frequency, the shorter the recording duration. (1200, 2400, 4800, 9600) |
| Stop delay | A button to set stop delay. It refers the duration, in seconds, of the recording after the trigger event. Maximum limit is 10 sec and available. |
In section Trigger, user selects the desired trigger from the list of trigger event.
Sampling Frequency (hz) | Number of Register in Sample | Size of Datalogger file (s) |
|---|---|---|
| 1200 | 8 | 13.6 |
| 16 | 6.8 | |
| 32 | 3.4 | |
| 2400 | 8 | 6.8 |
| 16 | 3.4 | |
| 32 | 1.7 | |
| 4800 | 8 | 3.4 |
| 16 | 1.7 | |
| 32 | 0.85 | |
| 9600 | 8 | 1.7 |
| 16 | 0.85 | |
| 32 | 0.425 |
The Data Logger Pro allows current and voltage waveform, alarms, and digital signals data associated with an event to be recorded. An SD card installed on the circuit breaker is necessary for this functionality, enabling longer recording durations. Additionally, the Pro version provides more variables compared to the basic version, offering a comprehensive overview of system events.
Prerequisite:
When all the prerequisites are satified, the Datalogger Pro section will appear. Click on the Options button to perform the configuration.
By accessing the "General" section, parameters such as the number of registers in sample, sampling frequency, stop delay and the enabling of datalogger can be set.
| Element | Description |
|---|---|
| Datalogger enabled | Enable/disable datalogger functionality |
| Number of register in sample | Number of register in sample (8, 16, 32,64) |
| Sampling frequency | Frequency of data collection. The higher the sampling frequency, the shorter the recording duration. (1200, 2400, 4800, 9600) |
| Stop delay | Set the stop delay, which is available only if "Single trigger" modality is selected. It refers to the duration, in seconds, of the recording after the trigger event. Maximum limit is 10 seconds. |
In the"Trigger" section there are two modalities available, "Single Trigger" or "Multi trigger". The latter one enables the possibility to set up to three different triggers.
Single Trigger
In Single trigger modality, you can set the Trigger type from the list of pre-defined trigger events or even a customized one according to your needs.
Multi Trigger
In Multi trigger modality, you can set trigger types independently for up to 3 triggers. A maximum of 30 total trigger events can be recorded during a single registration.
| Part | Description |
|---|---|
| Trigger modality | Enable multi trigger modality. |
| Trigger | Select the trigger you wish to set. |
| Trigger type | Set the type from the list of the trigger events. There is an option to set a customized trigger event as desired by selecting custom trigger type. |
| Register value | Set the trigger event type by hex decimal number |
Download a recording
Click on Download Datalogger and you will be presented with a window containing dedicated sections to be filled and selected.
| Filename | Choose the name of the datalogge file and the directory. By default file name is in CBTagName_Datalogger_YYYYMMDDhh:mm:ss format. File extension must always be ".abb" . |
| Trigger offset selection | Allows you to select the trigger event to be downloaded in case the Multi Trigger modality is chosen. |
| Free offset selection | Provides a cursor on the timeline with which you can choose at which timestamp to start the download operation. It allows the download window to be centered on an absolute time. Available when the Multi Trigger modality is chosen. |
| Time window | Time-based window for selecting the start and end of the Download. You can reduce or enlarge the window by scrolling the two cursors. |
The Datalogger file can be downloaded in two distinctive ways:
By unmounting the SD card from the breaker and connecting it directly to your PC. To perform this type of action, the circuit breaker should be in an opened state and the operation must be performed in full safety.
If you choose the second option, there would be no need to download the data on the Datalogger PRO, because you could open the recording directly in the Dataviewer tool by cliking on the "Open Card" button . The maximum DataLogger file size in seconds downloadable through Ekip Connect without unmounting the SD card is defined by a precise combination of the number of registers and frequency used:
| Frequency | Register | Size (s) |
|---|---|---|
| 1200 | 8 | 218.453 |
| 16 | 109.227 | |
| 32 | 54.613 | |
| 64 | 27.307 | |
| 2400 | 8 | 109.227 |
| 16 | 54.613 | |
| 32 | 27.307 | |
| 64 | 13.653 | |
| 4800 | 8 | 54.613 |
| 16 | 27.307 | |
| 32 | 13.653 | |
| 64 | 6.827 | |
| 9600 | 8 | 27.307 |
| 16 | 13.653 | |
| 32 | 6.827 | |
| 64 | 3.413 |
If you wish to download Datalogger files that exceed these limits, you should unmount the SD Card and connect it directly to your computer. Afterwards, you can read its data by accessing the Dataviewer tool.