Introduction

Cybersecurity tab

The cybersecurity tab will appear in the side menu if one of the following two conditions is met:
  • A Cybersecure device is connected.
  • The user has at least one role for Cybersecure devices.
 
Please note that, at this time, only Emax 3 devices are available in Cybersecure mode. Click here to learn more.
 
Within this section, the user will be able to view all the Cybersecure devices for which he has visibility.
For each device the user will be able to see some information and, based on the role he has for that device, he will be able to carry out some operations.
 
Cybersecurity devices page

 

If a Cybersecure device is connected, an orange dot will appear above the icon. 

Orange dot icon

 

In the left section (A) the user will see the information of the devices, such as Tag Name, Serial Number, Plant, together with the info regarding user's role on the specific device and the validity range of dates, when available.

In the right section (B) the user will see all the actions available on the device; these actions may vary based on the user's role for that device and whether the device is connected or not.