IO

Page functions

  • Configure the inputs and outputs of the device.
 

What it looks like

dashboard
 
PartDescription
Status
Status of inputs/outputs
on button icon: enabled
off button icon: disabled
ConfigurationInput/output configuration parameters
read iconButton to read the configuration from the device
download  iconButton to transfer the configuration to the device
 
Edit a parameter
  1. Expand the set of input/output parameters to be set.
  2. To read the saved values from the device, click on read  icon .
  3. Set the desired value/option.
  4. To transfer the set values to the device, click on download icon: a message appears with the result of the operation.