Load Shedding: what it looks like

Page Design

Page Design
 
Part
Description
A

Function Load Shedding area. It contains the following elements:

  • command to enable and disable the Load Shedding function
  • button Configure to display and change function parameters in Load Shedding in [C].
  • (only for Adaptive load shedding) button Configure to display the parameters of the solar system in [C].
  • (only for Adaptive load shedding) button Configure to view the parameters of the Automatic Transfer Switch in [C].
B

Loads area. It contains the following elements:

  • graphical representation of each load (Graphical representation of the load)
  • (only for Adaptive load shedding) button Supervision to access the Supervision page (Page Supervision)
  • button Add new load to add a load
  • button Breakdown to open another project or create a new project
  • button Reset alarms to reset the alarms of all loads, visible on the page Supervision.
  • button Save project to save the project on the PC in .lds format.
Note: the .lds format is a proprietary format that can only be read with Ekip Connect.
  • button Transfer to transfer the configuration to the device
CArea for the parameters of the element selected in [A] or in [B] (Load Shedding: parameters)
 

Graphical representation of the load

Power controller
 
Part
Description
AAssigned disconnection priority
BIcon selected for the load
CName assigned to the load
D

Load configuration status:

  • Completed: all necessary parameters have been configured
  • Not completed: one or more necessary parameters not configured
settings iconButton for customising the load icon
icon To display the button, position the mouse pointer over the graphic representation of the load.
close icon
Button to delete the load
icon To display the button, position the mouse pointer over the graphic representation of the load.
 

Page Supervision
Note: page only available for Adaptive load shedding.

 
Adaptive load shedding
 
Part
Description
CommissioningButton to access the Design page (Page Design)
A

Load status area.

  • The following information is provided for each load:
  • presence of alarms
  • signal status
  • load status
BGraph: time (X-axis) and power (Y-axis). Displays the estimated power generated by the photovoltaic system during the year.
 
CFrequency measured in real time