Download Latest Version here: Ekip Connect
Emax 3 Cybersecure Role Based Access Control management
Custom Logic Main-Tie-Main Closed Transition Templates
Import of Protection Parameters from Sace Emax 2 to Sace Emax 3
Purchase device Test reports directly on Ekip Connect.*
New wizard to change the Circuit Breaker Execution parameter.
Double click on any slider in Ekip Connect to insert the desired value via keyboard.
Added specific separator for thousands in order to distinguish it from the decimal values in the Measuring Page.
New device M4M 32 integration and configuration
Possibility to report an issue alongside the device settings report directly to the ABB support team
Dashboard, introduced a visual percentage graph on the Measures page to provide easier data interpretation
Redesigned the Tools view in groups with clear labels
Redesigned Test Area tool
Role Request, added Device Families description
New Download log feature in the Options menu
Improved Send Frame TCP communication [Internal R&D only]
Improvements
Improvements
Fixes
Improvements
Fixes