Introduction

Device pages

For the communicating device, Ekip Connect displays pages for configuring and monitoring the device. The pages contain information and commands specific to each device. Where applicable, please refer to the device documentation.
The pages display parameters and values graphically. The Classic view page shows the parameters and values from the other pages and, for some devices, also additional parameters, in list mode.
 

Note on the images

The images of Ekip Connect shown on the following pages are examples for the device category.
 

Overview

For each page, the following table shows the categories of devices that require that page. If it is not required for all devices, a number of devices are shown by way of example. To find out which devices belong to each category, see List of devices per category.
>> For details on the pages enabled for each individual device, please refer to document 9AKK108467A9237 available here.
PageExternal unit for circuit breakers
Circuit breakers
Energy metersStationFuse-disconnectors, change-over switches
DashboardxxM4Mx-
Informationxx-x-
ConfigurationxxM4Mx-
MonitoringxxM4ME-Hub 1.0-
IO setup---E-Hub 1.0-
Protectionsxx- -
Communication---E-Hub 1.0-
Connectivity---E-Hub 2.0-
Modulesxx-E-Hub 2.0TrueOne Touch
IO--M4M--
Notifications--M4M--
Classic viewxxxxx
 
 

List of devices per category

CategoryDevices
External unit for circuit breakersEkip UP
Ekip UP+
Circuit breakers
XT
Emax2
CSU-2
TVOC-2
SSCB
Energy meters
EQmeter
InSiteProM
M2M
M4M
EQmatic
IM300-U
IM300-I
IM301
IM302
IM303
EM400
CMS700
StationE-Hub 1.0
E-Hub 2.0
Fuse-disconnectors, change-over switches

TruOne
TruControl

Slim line XR ITS 2.1