Reports

The Reports function allows you to generate, print and download the following documentation:
  • the Settings Report, which is a report containing all the information contained in the device memory, and thus also with the values of all the parameters set and measurements recorded on the device connected.
  • the Factory Report, which is a report made by the factory after the manifacturing process of on your device regarding some specific tests

Setting Reports

Access to the functionUnrestricted
Type of devices that support the function
  • External unit for circuit breakers (e.g. Ekip Up)
  • Circuit breakers
  • Energy meters
  • Station
  • Fuse-disconnectors, change-over switches
Device statusConnected and communicating
Type of connection with the deviceConnection via Ekip T&P, serial network (Modbus RS485) and Ethernet (Modbus TCP)
>>For more details on supported devices and requirements for each, please refer to document 9AKK108467A9238 available here.
 

What it looks like

settingsreport
PartDescription
A
  • Open: it opens a report previously downloaded and saved on the PC
  • New: it generates a single report of the device connected
  • New Collection: it generates multiple reports for each device connected
BField to search for a report by name
C

List of Settings and Factory reports generated. The following information is provided for each report:

  • Report name
  • Type and customised name of the device
  • Report generation date and time
  • Action buttons:
    • Close icon: deletes the reports
    • csv: downloads the report in .csv format
    • pdf: downloads the report in .pdf format
    • displays the report icon: displays the report
 

Generate a report

  1. With the device connected and communicating with Ekip Connect, click on Tools > Reports.
  2. Click on New.
  3. Enter the name of the report, for example, the name assigned to the device in the installation.
  4. Click on Save report: Ekip Connect generates and displays the report of the information in the device memory.
  5. If required, download or print the report.
 
View a report
  1. In Tools > Reports, identify the required report. If necessary, use the search field
  2. Position the cursor on the relevant line of the report: the report action buttons appear.
  3. Click on Open icon: the report opens.
 

Open a report saved on the PCIn Tools > Reports, click on Open and select the .pdf or .csv file of a report previously generated and downloaded with Ekip Connect: the report opens.

 
IMPORTANT: the data visible in the report depends on the role of the user viewing it

Factory reports

Access to the functionUnrestricted
Type of devices that support the function
Circuit breakers
 

What it looks likefactoryreports

factory-report-massive1
factory-report-massive2
PartDescription
A
  • Open: it opens a report previously downloaded and saved on the PC (internet connection is required)
  • Download: it opens the window shown in the part C below 
B
Form to fill with the Serial Number and the Commercial Code of the devices requested
C
  • Next: go to the summary page of the factory tests selected
D
Summary page of all the factory tests selected with their corresponding download result