Read the previous article
Power Controller: useful information
Part | Description |
|---|---|
| A | Function Power Controller area. It contains the following elements:
|
| B | Loads area. It contains the following elements:
Note: the .pwc format is a proprietary format that can only be read with Ekip Connect.
|
| C | Area for the parameters of the element selected in [A] or in [B] (Power Controller: parameters). (only if selected Power Controller in [A]) Button to open the Window Power Controller programming |
Part | Description |
|---|---|
| A | Assigned disconnection priority |
| B | Icon selected for the load |
| C | Name assigned to the load |
| D | Load configuration status:
|
| Button for customising the load icon | |
| Button to delete the load |
Part | Description |
|---|---|
| Week summary | Button to show/hide in [B] the programming of the entire week. In this view, programming cannot be changed. |
| Add time slots | Button to add a time slot to the programming. |
| Remove time slot | Button to remove the last added time slot from the programming. |
| A | Commands to select the day of the week to be displayed and buttons to scroll through the days. |
| B | Programming display area.
|
| C | Command to define the programming of a day based on the programming of another day. |
| D | List of defined power limits. Up to 10 power limits can be set. |
| Part | Description |
|---|---|
| Commissioning | Button to access the Design page (Page Design) |
| A | Load status area.
Button Clear Alarms to rest the alarms of all the loads. |
| B | Graph: time (X-axis) and power (Y-axis). Displays the power limit value set for that period, the average power value recorded and the estimated average power value. |