Modules

Page functions

  • Configure additional modules of the device.


What it looks like (IO module)

IO Module
Part
Description
AImage and device information
B

Pages menu:

  • Analog: page for configuring analog inputs
  • Digital: page for configuring digital inputs
C

Inputs area. The following data are shown for each input:

  • Customisable name
  • Input type
  • Sensor data that have been set (minimum and maximum value and unit of measurement).
  • delete icon: Removes the sensor from the input.
  • Modification: changes the input and sensor parameters.
  • Add sensor: displays area [D] to configure the input and the associated sensor.
D

Parameters area. The following are the most significant parameters:

  • Unit: sensor measurement unit
  • Pulse amplitude: increment value
 

Associate a sensor with an input

  1. Select Analog or Digital: the relevant input configuration page opens.
  2. Click on Add sensor: the input is populated with default values.
  3. Click on Modification and in the editing area, set the parameters.
  4. To save the changes, click on Save: a message appears with the result of the operation. Or to cancel, click on Discard.