Monitoring

Monitoring page functions

  • View historical data measured.
  • View data measured in real time.
  • View power quality data.
  • Reset imported and exported energy meters.
 

What it looks like

monitoring page
 
PartDescription
AMonitoring pages menu
BPage-specific data
CPage-specific menu
 

Page Energy > Overview

energy meters
 
PartDescription
AMenu to display imported and exported energy values
Active energyActive energy values per phase and totals, imported or exported, depending on what is selected in [A]
Reactive energyReactive energy values per phase and totals, imported or exported, depending on what is selected in [A]
Apparent energyApparent energy values per phase and totals, imported or exported, depending on what is selected in [A]
TariffsActive energy values, imported or exported, depending on what is selected in [A], broken down by tariff
Reset energy countersButton to reset energy meters
 

Reset energy meters

  1. From the menu, select the type of energy (imported or exported) you want to display.
  2. Click on Reset energy counters: the selected energy meters are reset.
 

Page Energy > Cumulative

cumulative energy
 
PartDescription
A
download icon: downloads all cumulative energy data stored in the device memory in Excel format.
reads icon : reads the data from the device memory
BReference period, minimum and maximum value with the timestamp of the selected parameter
CGraph with the energy consumption curve for the selected parameter
DList of available parameters
 

Page Energy > Trend

energy trend
 
PartDescription
A
download icon: downloads all energy data stored in the device memory in Excel format.
read icon: reads the data from the device memory VCLA.
BReference period, minimum and maximum value with the timestamp of the selected parameter
 CGraph of energy values stored during the defined time period (difference between the value at the beginning and end of the interval)
DList of available parameters
 

Page Power quality > Overview

Power quality
 
This area shows the following values:
  • Line voltage THD
  • Phase voltage THD
  • Current THD
  • load unbalance
  • power factor
  • phase-shifting factor


Page Power quality > Harmonics

 Page Power quality > Harmonics
 
Part
Description
A

Harmonic type menu:

  • line voltage
  • phase voltage
  • currents
BGraph up to the 40th harmonic of the type selected in [A].
The vertical axis indicates the amplitude of the harmonic expressed as a percentage of the fundamental harmonic. By clicking on the graph, the value of the specific harmonic can be read.
 

Page Request

Page Request
 
PartDescription
AIcona download: downloads all minimum and maximum values stored in the device memory in Excel format.
BMinimum and maximum values of the selectable parameter. Depending on the device configuration, up to three levels of minimum and maximum values are available.
CList of available parameters
 

Page Load profile

Monitoring meters loadproof
PartDescription
A download icon: downloads all load profiles stored in the device memory in Excel format.
BReference period, minimum and maximum value with the timestamp of the selected parameter
CGraph with load profile curve for the selected parameter
DList of available parameters