Configuration

Page functions
View and edit device parameters in relation to the installation where the device is installed.
View and edit some internal configuration parameters of the device.


What it looks like

configurationview
 
Part
Description
AExpand icon: expands all parameter sections.
collapse icon: collapses all parameter sections.
BText search area for parameters
CParameters section
expand icon: expands the parameters section.
collapses icon: collapses the parameters section.
DButton to apply or cancel chang
 

Edit a parameter

  1. To view all parameters, click on Expands icon.
  2. Set the desired value or option.
  3. To transfer the change to the device, click on Apply: a message appears with the result of the operation.
Note: if the operation fails, check the status of the operating mode (Operating mode).