Load Shedding: procedure

Configure the function Load Shedding

  1. Click on Tools > Load Shedding.
  2. To start a new project, select the chosen version of Load Shedding or select the button to read the configuration Load Shedding active on the device.
 load shedding configuration
  1. Enable the Load Shedding function and click on Configure to configure the function parameters.
  2. If there is a solar system and/or ATS, click on Configure corresponding to the element in order to configure the necessary parameters.
  3. Add as many loads as there are loads in the system to be monitored.
  4. Set the parameters for each load (Load Shedding: parameters).
  5. To save the project, click on Save project.
  6. To transfer the configuration to the device, check that the device is connected and communicating with Ekip Connect and click on Transfer: at the end of the transfer, a .pdf file containing the configuration report can be downloaded.
Note: to transfer the configuration to the device, you must have activated the purchased package on Marketplace.
 

Monitor the function

  1. With the device connected and communicating with Ekip Connect, click on Tools > Load Shedding.
  2. Open a project or select the button to read the configuration Load Shedding active on the device.
load shedding configuration
  1. Click on Supervision.