Dashboard

Page functions

  • Display the summary or most critical information for the device
  • Access pages with more detailed information.
 

What it looks like

Dashboard page
 
 

Area Measurements

Area Measurements: Currents

 

Area Measurements: Voltages
 
Area Measurements: Powers
 
PartDescription
AButton to access the Measurements section of page Monitoring
BMeasurements menu
C

Current measurement display area

  • Current RMS: measurements acquired:
    • Current of each phase
    • Ine: neutral current
    • IGnd: internal earth fault current
    • IGndEx1: external earth fault current
  • Max. current value: maximum phase current measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Min. current value: minimum phase current measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Reset: button to reset minimum and maximum values
D

Voltage measurements display area

  • Voltages RMS: measurements acquired:
    • voltage of each phase (single and line-to-line)
    • U0: neutral voltage
  • Max. voltage value: maximum phase voltage measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Min. voltage value: minimum phase voltage measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Reset: button to reset minimum and maximum values

E
Power measurements display area:
  • phase and total active power
  • phase and total reactive power
  • phase and total apparent power
 

Area Events

Events area
 
PartDescription
AButton to access the Events section of page Monitoring.
B

Events menu:

  • All: displays the last six events recorded, excluding trips and alarms
  • Interventions: displays the last six trips recorded.
  • Alarms : displays the last six alarms recorded.
C
Area that displays the events selected in [B]:
status change icon: status change
warning icon/Icona di attenzione disabilitata: warning
error icon: error
information icon: information
edit icon: change
Area Status widget

Area Status

PartDescription
Circuit-breaker state
closed icon: closed
open icon: open
undefined icon: undefined
Circuit-breaker trip
tripped icon: tripped
not tripped icon: not tripped
Contact wear0% = no wear
100% = completely worn
# OperationsTotal number of manual operations, interventions, failed interventions and test interventions.
 

Area Information

 
information area
PartDescription
AButton to access the Information page
BCustomised device name (parameter CB Tag name editable in Classic view > Unit configuration > Customisable information)
C
Device type (parameter CB Type also visible in Classic view > Information > General parameters)
DNumber of poles
ERated current (In)
FRated voltage (Un)
GFrequency
 
Reset the minimum and maximum recorded values
Note: function only available if the device is connected to Ekip Connect via a point-to-point connection.
 
  1. In Measurements, click on the measurement type (Currents or Voltages) for which you want to reset the minimum and maximum values.
  2. Click on Reset.