The Diagnostic function allows you to check the flow that the device performs to collect data from the field and transmit it to the cloud.
Requirements
Access to the function
Unrestricted
Type of devices that support the function
Gateways, External units for circuit breakers, Fuse-disconnectors, change-over switches, Circuit breakers (with Ekip Com Hub communication module installed)
Device status
Any
Type of connection with the device
Connection to Ethernet network (Modbus TCP)
>> For more details on supported devices and requirements for each, please refer to document 9AKK108467A9238 available here.
What it looks like
Part
Description
A
Buttons on the page
Start/Stop: starts/stops the diagnostics session.
Repeat Selected Tests: repeats the selected tests.
Generate Report: allows the session report to be saved in .pdf format
Show Log: displays the diagnostics session logs.
Configure TCP Scan: opens the window to set the Ethernet TCP network scanning parameters
C
Session test list:
: test running
: test completed successfully
: test completed with problems
Details: shows additional information about the test.
Perform a diagnostic session
Click on Configure TCP Scan: the Device scan settings window opens.
Set the parameters of the Ethernet TCP network to which the device to be tested is connected and click on OK.
Click on Start: a window appears asking you to enable the configuration session on the device.
Manually enable the session on the device, then click on OK.
If requested, in the Select Hub window, select the device to be tested.
In the ABB Ability ENVIRONMENT window, select the usage environment, then click on OK: the Log in window appears.
Log in: the Hub Password window appears with the serial number of the device already filled in.
Enter the 16-digit password of the device, then click on OK: the results of the tests performed appear.