Read the previous article
Load Shedding: what it looks like
Element | Description |
|---|---|
| Enabled | Includes/excludes the load from the function algorithm |
| Name | Name assigned to the load |
| Power consumption | Rated power of the load |
Disconnection priority | Position of the load in the load disconnection sequence. Priority 1 corresponds to the first load to be disconnected. |
| Element | Description |
|---|---|
| Signal status/Commands > Contact | Device cable used for signal.
|
| Signal status > Meaning | (only if the device used for the signal is a circuit breaker and the optional status signal is activated).
|
| Signal status > Polarity |
|
| Signal status > Delay | Delay in seconds before the signal is processed after reception |