Introduction

Foreword

Ekip Connect can connect to several devices simultaneously but only communicate with one device at a time.
 

Available scans

 

Connection type
DescriptionProcedure
T&PScan via USB Flash Drive by means of the Ekip T&P or Ekip Programming converter.Scanning via ABB key
USB-CScan via USB-C cable  
SerialScan that looks for devices connected via serial network.Serial bus scan
EthernetScan that searches for devices connected via an Ethernet network. Each device is recognised via an IP address.Ethernet network scan
Manual
Scan with manual definition of parameters and Modbus connection method.
Especially useful for devices without SlaveID (identifier for communication between devices ABB S.p.A)
Manual scanning
Note: when using the software for the first time, it is recommended to use a connection via USB (Ekip T&P or Ekip Programming).
Note: devices can be connected via BLE (Bluetooth Low Energy) through the EPiC app. For more information, please refer to the app documentation available here.
 

Device information on page Scanning

In section Devices found, the devices found after scanning are listed. The following information is provided for each device:
deviceinformationscanning
PartDescription
A
Device status:
  • found but connection not yet established icon: found but connection not yet established
  • connected icon/connected icon (alternately): connected and operating normally
  • active alarms icon/active alarms icon(alternately): connected but with active alarms
  • error icon :disconnected
 
Note: a disconnected device remains visible until the next scan or a restart of Ekip Connect.
B
Device family identifier, Tag Name and Serial Number
 
Note: the parameter Tag name is editable in Classic view > Unit configuration
CIP address and/or port used for connection and its configuration
D
  • CONNECTED: device connected and communicating
  • SELECT: button to enable communication with the selected device
 
Note: Ekip Connect can only configure and monitor one device at a time. Enabling communication with the selected device inhibits communication with the previously enabled device.