Monitoring

Monitoring page functions

  • View the measured data
  • Display recorded events, alarms and trips of the protections.
 

Page Measurements

Measurements page
 
 
PartDescription
AMonitoring pages menu
Currents

Current measurement display area

  • Current RMS: measurements acquired:
    • Current of each phase
    • Ine: neutral current
    • IGnd: internal earth fault current
    • IGndEx1: external earth fault current
  • Max. current value: maximum phase current measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Min. current value: minimum phase current measured. Value calculated since power was supplied to the device or since the last manual reset.
  • peak factors of each phase and neutral
  • graph of load profiles
Voltages
Voltage measurements display area
  • Voltages RMS: measurements acquired:
    • voltage of each phase (single and line-to-line)
    • U0: neutral voltage
  • Max. voltage value: maximum phase voltage measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Min. voltage value: minimum phase voltage measured. Value calculated since power was supplied to the device or since the last manual reset.
  • Reset: button to reset minimum and maximum values
FrequencyFrequency measurement
Power factorPower factor measurement
Power

Power measurements display area

  • phase and total active power
  • phase and total reactive power
  • phase and total apparent power
Energies
 
 

Page Alerts

alert signal
 
PartDescription
AMonitoring pages menu
Interventions    Display of the last five recorded trips in a continuous sequence
AlarmsDisplay of the last five recorded alarms in a continuous sequence
AlertsDisplay of the last five recorded warnings in a continuous sequence
Most frequent trip events    
Display of trips by type of protection that caused the trip during a given period (last week, last month, last year, all)
Number of trips: total trips in the selected period
Shows all trips: link to page Trip (Page Interventions)
 

Page Events

events page
 
PartDescription
AMonitoring pages menu
Events    

List of all recorded events, including alarms and trips. The following information is shown for each event:

  • type
  • name
  • recording date and time
  • duration
 

Page Interventions

intervention page
PartDescription
AMonitoring pages menu
Content
Interventions    
List of trips recorded The following information is provided for each trip:
  • the protection that caused the trip
  • date and time of the trip
  • the measurements associated with the tripped protection
  • state of wear of the contacts (0% = no wear, 100% = completely worn)